This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61169: Number of "LED strings" can this part drive in parallel

Part Number: TPS61169
Other Parts Discussed in Thread: TPS61500, LM3410, TPS61500EVM-369

Hi 

I have an application that requires drive upto 200 LEDs in a constant current mode, the voltage source is a single cell rechargeable LiPo battery.  The "LED string" has the following parameters

LED Voltage drop ~1.67V to 2V

LED string current 15mA

Total number of LEDs 200

My questions are the following:

1. Is this part suitable or is there a more suitable part

2. What is the optimal number of LEDs per string