This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910: VMMC re-start behavior

Part Number: TPS65910

Hi,

Does VMMC start up normally under these conditions?

①Write 00b to address 0x35 to set VMMC in SLEEP state.
②The device turns off.
③Supply power again and the device turns on.

In our customer's application, turn off VMMC to transition to backup operation in the event of power failure.
After that, the power is turned off while VMMC is off.
If the power is turned on again in that state, will it start up in the normal power sequence?

Best regards,
Yuto Sakai