This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5160A: Design viability for two outputs 24V and 5V

Expert 4640 points
Part Number: LM5160A
Other Parts Discussed in Thread: LM5160

Dear e2e,

I'm looking for the best option for the following requirements:

28Vin (ideally 20V to 80V) --> 24Vout@100mA & 5Vout@1A

Considering the "low" output power, I thought that the LM5160A could fit, in a flybuck topology; but it seems that the recommended duty cycle of 50% can't be applied here...

Do you confirm?

Could you recommend any other TI part and topology (flyback?) ?

Regards,