Part Number: LM5160A
Other Parts Discussed in Thread: LM5160
Tool/software: WEBENCH® Design Tools
Hi,
I have a problem with the design I did in the WEBENCH for the component LM5160 .
I use the LM5460 component as an isolated DC/DC to convert from 28v to 5v isolated with an output current of up to 1.5A.
The following is the design result I received from the WEBENCH:
The problem is that during the POD to the board with the dc/dc design according to the WEBENCH, as soon as I connect a load that draws a current of 300mA, there is a voltage drop from 5v to 4.5v.
the design is for 1.5A current consumption, what the problem?