This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5907: P2P to PT5108

Part Number: LP5907

Hi team,

  1. Do we have suitable LDO for P2P to replace fixed output version of LDO of PT5108? The output voltage is required to be 1.8V, 2.8V and 3V, and the price is as low as possible.
  2.  It is used in the Thermostat of household air conditioner.
  3. At present, I choose LP5907. Can I use LP5907 to replace PT5108 this one?
  4. Do you have any better recommendations?

 

Best Regards

Wesley Huang

wesley-huang@ti.com

  • Hi Wesley,

    The LP5907 is the better than recommendation:

    1. Lower IQ

    2. Lower Noise

    3. No Need for external Bypass capacitor (they can keep this as the this is an NC pin on the LP5907)

    I hope this helps.