Other Parts Discussed in Thread: DRV8313EVM, , DRV8313
The data sheet for this part on Page 15, paragraph 8.2.2.2 spec's that the output cap needs to be tantalum (based on requirements) but it goes on to say a ceramic MLCC can be used with a series resistor of 500mOhm to 1Ohm. However, the development board DRV8313EVM, which appears to be the only eval board with this part, shows in the schematic DRV8313EVM_SCH the use of a TDK ceramic cap C2012X7R1A106M without such a series resistor. Is this in fact a proper application of a ceramic capacitor, and in specific this TDK cap? Reason for this question is that as we all know tantalum cap prices are sky high and this ceramic cap is much cheaper, and the PCB is lay'd out without this series resistor. So I am looking for guidance here as to whether I need to change the PCB layout. The tantalum based application has worked flawlessly in fielded units. Thanks in advance.