I've got a circuit using the BQ25886 with a 100mA to 600 ma load on Vsys. In addition, I have a couple of 16450 batteries
attached to Vbat. If everything is hooked up, Vsys is at 8.4 VDC. If I pull out one of the batteries so that VBAT goes to
zero, the charger starts to cycle Vsys. This phenomenon occurs irrespective of whether I use a laboratory supply or
a USB converter.
I have the D+ and D- lines shorted together (not connected to anything else).
This phenomenon was reported by "ajayt", and you responded by saying that Vsys should drop to Vsys_min, which is specified at 6.2 V (min.)
In my case, Vsys is dropping below 4.0 V.
Can you provide some help in troubleshooting this?
Thanks