Other Parts Discussed in Thread: TPS54540
I am designing a PSU PCB with 3 different rails, but I’m unsure where to position the layouts for each of the 3 rails for best results.
Up the top are 3 black lines representing the rails that the external devices will draw their current from. I want to have the components and most circuitry on the top layer, and the bottom layer reserved for a universal ground plane.
Rail 1: +12V @ 3A
- LMR14050
- large output current
- Needs to be low noise
- doesn’t add a large amount of switching noise to rail
Rail 2 +5V @ 1A
- LMR14050
- low output current
- can be higher noise
- doesn’t add a large amount of switching noise to rail
Rail 3 -12V @ 1.5A (buck-boost-inverter)
- TPS54540
- large switching current
- needs to be low noise (preferably same as +12V)
- Has a larger amount of switching noise on rail due to BBI design.
Some restrictions:
- position of output rails, power input and board size/shape can not be changed.
- Board is limited to 2 layers.
- all components must be on the top layer
So my Question is:
Where should I position each rail for lowest noise on the +/-12V rails? (considering that the +15V power and ground inputs are on the bottom left of the PCB)