Hi,
Customer is asking following question:
In TPS2662’s datasheet, figure 30. timing waveforms. It seems that eFuse asserts fault if current through input to output is below 31mA (15mV/478mohm).
Can you confirm that ?
If it so, we can’t use FLT-pin to enable DC/DC after the eFUSE, because the “low current” fault will shut down the DC/DC with idle current.
I just ask to make sure, does it behave like this?
Thanks & BR,
KF