I am developing a design using two LM76202-Q1s in a diode-OR configuration. The inputs to the two units are potentially independent (for redundancy), depending on end-user wiring harness configuration.
Should the RTN plane of each LM76202 be separate, or is it acceptable to join the planes to create a single RTN plane? Are any protections sacrificed if they are joined? The motivation for joining them would be for increased thermal dissipation in the critical case of one unit taking the full current load.