This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can the TPS65131EVM-063 operate under these conditions?

Other Parts Discussed in Thread: TPS65131, TPS63700

Hi:

We want to use TPS65131EVM-063 Evaluation Module ,

we have the some condition below

input=3.0V~3.6V

Output= positive voltage ~18V; negative voltage ~ -15V

and output current neet  ~500mA(or higher)

Could this EVA board support our request?

Please kindly reply me, thanks.