This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59116: LED Driver with a single power supply

Part Number: TLC59116

Hi, team.

The customer is considering TLC59116, but requires two power supplies for VCC and VLED.

It is disadvantaged because the competition can operate with a single power supply.

Have you developed an LED driver that can operate with a single power supply?

 LED current is 20mA
 Four LEDs in series for each line
 VLED is about 15V

Best Regards,