This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27712-Q1: Gate Driver output current | Gate driver supply current | Decoupling capacitor current

Part Number: UCC27712-Q1

Hi,

I have a couple of questions. Could someone please help me?

Question-1. I want to simulate a buck converter using this gate driver IC. Can I get the TINA model or the SPICE model of it?

--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

Scenario:

I have the gate driver and MOSFET whose gate charge is 26.5nC and let the charging time be 100ns or 50ns (Switching frequency = 500kHz, duty cycle = 0.3), based on which I get a I_average = 110 mA, let the peak current required is 2 A sourcing and 1.5 A sinking,

My voltage source can supply supply 10mA to the gate driver continuously.

If I design and use the decoupling capacitors at the gate IC supply, will the complete gate current be supplied by decoupling capacitors? Will there be any problem from the source voltage being loaded?

Please help me clarifying this detail.

Thanks,

Subbu.