This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170EVM-BIDIR: LM5170 boost mode issue

Part Number: LM5170EVM-BIDIR
Other Parts Discussed in Thread: LM5170, LM5118

Hi Team,

My customer is testing LM5170 EVM-BIDIR  boost mode function but doesn't get output voltage. the test process is below,

1. HV48VDC port is connect to DC load

2. J21 pin 1 & 2 closed

3. J4 pin 1 & 2 closed

4. J34 pin 1 & 2 closed

5. J35 pin 1 & 2 closed

6. J36 pin 1 & 2 closed

7. J37 pin 1 & 2 closed

8. J14 pin 1 & 2 closed

9. J15 pin 1 & 2 closed

10. J19 pin 1 & 2 closed

11. J29 pin 1 & 2 closed

12. J30 pin 1 & 2 closed

13. J28 pin 2 & 3 closed

14. J31 pin 1 & 2 connect to 5V

may we check what else we missed?

Thanks 

Eddie Chou

  • Hi Eddie,

    Thank you for posting.  It's better if you send me a photo picture of board so I can quickly check if the jumper is used correctly.  The list is harder to follow.

    J14, J15, J19 are not needed, and J31 is not clear: where does the 5V come from?  The EVM's 5V rail or external 5V?  

    Anyway, I think you did not follow the User Guide nor read the datasheet circuit breaker section.  The circuit breaker only operates when the 48V-port has a voltage at least 10V higher than the 12V-port voltage. You just have a load, then the breaker cannot be turned on.  Also, in the User Guide section 3.2, the second step is:

    2. Turn on the HV-PS power supply and HV-E-Load.

    This HV_PS is to turn on the circuit breaker at the beginning. Once the boost operates, this supply can be removed.  You do not have a supply there, so this won't work.

    In order to run the EVM as a regular boost converter, you need to do the following: 

    1. Solder a copper strip (able to conductor at least 60A) to the two exposed pads beside D3 on the back side, to bypass the circuit breaker. 

    2. Solder an 100k resistor to R4 (below J1).  This is to provide an onboard UVLO control.  Once the input is supplied, the circuit will automatically start.

    3. Remove all jumper caps, then re-apply to close the following jumpers.

    Either J1 (2,3) or J1 (1,2) should work for boost mode.

    J3 (1,2)  To disable the fault detection because it if 48V-port is just a load.

    J4 (1,2)

    J5 (2,3)

    Either J21 (1,2), or J21(2,3), both should work for boost mode.

    Either J25 (1,2),  or J30 (1,2), but not both, to enable the CH-2

    J28 (2,3)

    J29 (1,2)

    J34 (1,2)

    J35 (1,2)

    J36 (1,2)

    J37 (1,2)

    If you want to run buck, change to the following jumper positions: J1 (1,2);  J21 (1,2); J28 (1,2). 

    Hope this clarifies.

    Thanks,

    Youhao

  • Hi Youhao,

    Attached is customer EVM setup photo, they are not able to boost both connect J31 to in 5V or external 5V. thanks.

  • Hi Eddie,

    The jumper positions look correct.  Has the customer soldered a copper strip to short the two exposed pads beside D3 on the back side? This must be done first in order to run boost mode with E-load. 

    Do you also check if 10V is produced by the LM5118 circuit on the upper right corner of the board?  You need 10V, 5V and 3.3V bias rails which should be produced by the EVM onboard circuits.

    Can you confirm?

    Thanks,

    Youhao