This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54160: cannot run the transient reference design downloaded from tina website

Part Number: TPS54160

I am trying to simulate the transient reference design downloaded directly from the tina website, but it seems to complain about the operating point not being found. I have read and followed what was suggested in other posts, and have also tried to implement the instructions given below the downloaded reference model, but none of it seems to work. I also noticed that I can only get some output when the input itself is below 2 V. 

Does anybody have any suggestions?

  • Krutarth,

    Did you download the TINA model from the TPS54160 "Design and Development" tab? What edits did you make?

    What version of TINA are you using?

    I downloaded the TINA model and have no issues running transient simulation of the default schematic with TINA 9.3.200.277

    Let me know,

    -Orlando