Other Parts Discussed in Thread: BQSTUDIO
Hello,
I have a bq2060a connected in a circuit and am communicating with it via EV2200 using 2200-60 Software. I am able to load the EEProm, calibrate voltage and current successfully, however when it comes to calibrating temperature, i run into an issue with accuracy. The range of values for the temperature offset per the datasheet is -12.8 through +12.7. The calibration occurs in Kelvin. I have a clean room that is set at 22.0C which is 295.2K. I follow the standard calibration procedures and after calibration the temperature will not budge from 375.2K. When reading the EEProm, the value is at the minimum allowance of -12.8. This is common on 45 boards so far.
Is there another software i can use with the bq2060a to calibrate the temperature? Maybe bqeasy or battery management studio? This design is old and is supporting an existing product.
Thanks
Ashley