This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27211: PWM Tina Simulation Question

Part Number: UCC27211


Hello,

I am fairly new to Tina. I am currently trying to simulate a Full-bridge DC/DC converter using two-half bridge GD, UCC27211. The expected output is Vo = 30V and Io = 3 A. Would I need single PWM controller or would the piecewise linear signals possible. Full Bridge_Phase1.TSC

  • Hi Raymond,

    Thanks for reaching out on e2e,

    Our high power drivers typically need a PWM input signal. Piecewise signals should be possible however to achieve the smallest propagation delay time and best input to output performance PWM is recommended. Let me know if this makes sense or you have any other questions.

    Thanks,