Hi,
The PN is TLV70230QDSERQ1;
We use TLV70230QDSERQ1, input 3.3V or 4V, measured output is 2V, EN is 2.8V, how many inputs should be set to get stable 3V / 300mA, does the circuit need to be adjusted? How to adjust?
Is there a corresponding table for input, output, and current?
This is also the case when no-load, not like the problem of overload;
Thanks
Elsa Duan