Dear Sir,
I want to set OTC(55c), OTCR(54c). Gap of OTC and OTCR is just 1c.
There are any effect to operation?
U6_25R Main PCB_V0.2(181025).pdf
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
I want to set OTC(55c), OTCR(54c). Gap of OTC and OTCR is just 1c.
There are any effect to operation?
U6_25R Main PCB_V0.2(181025).pdf
Thanks.
Does not have a IC tolerance?
Actually, I set the OTC (55 dgree C) and the OTCR (50 dgree C).
But now I want to change OTC and OTCR so closely.
And I consider about with thermistor and TI IC tolerance.
I use the thermistor tolerance is 1%(10㏀), then I want to asked about to gap with OTC and OTCR.
How much is proper value?
Hello Han Byu Lee,
The temperature measurement is based more on the tolerance of the NTC thermistor the customer uses.
We recommend a 103AT-2 Semitec, that's what we have on the EVMs.