Other Parts Discussed in Thread: TPSM53604
Hello,
There are two parts on my board and both need 3.3V.
Two parts are functionally separated but physically connected to each other by IO lines.
One part will control internal part and the other will drive and receive signals to/from outside of board.
Current consumption of one part will be about 3A. And the other will consume about 2.5A.
Is there any difference(pros and cons) between when one DC/DC(over 7A) converter is used and when two DC/DC(4A) converters are used?