This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5569: LP5569 LED Fault Detection Charge-up require

Part Number: LP5569
Other Parts Discussed in Thread: TIDA-01559

I am using a common Anode LED's and the circuit is very similar to your reference design "Capacitive Touch-Based User Interface with Proximity Sensing and LED Animation Reference Design TIDA-01559". The only difference we are powering with a 5V source. 

Since the charge pump output is not used to power the LED, Can we still use production-level testing of Short and open circuit detection?

If so do I still need to enable the Charge pump 1.5X mode during Open LED test and 1X Mode during Short LED Test, even when I am not using the charge pump output of the device.