This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3488: Control loop stability

Part Number: LM3488
Other Parts Discussed in Thread: LM5122

Hello, I develop power source for a heating (input 12 V, output :8A, 24 V;Fswitch 500kHz). But i don't undurstand how to design control loop. i can't found correct values for R6, R7 and C9. For configuration of the scheme presented in PDF output voltage is only stable 22 V (but divider is designed for 25 V in this config) on load around 8 ohms How i can calculate R6, R7 and C9 values? Datasheet don't contain information about it, it has only 2 reference design.7802.DC-DC.PDF