This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65130: Duty Cycle Min & Max

Part Number: TPS65130

Hi there, 

Are you able to provide any more information on the min and max duty cycle specifications? Do these specifications follow a production spread? Whether the delta is 0.5% from typical or 5% from typical heavily dictates the minimum or maximum output voltages possible for a given input voltage. 

Thanks, 
Shaun