Dear Sir,
Could you please confirm below ①② about the "TRM SLUUBB0?December 2015 Page16 3.3 I 2 C Command Waiting Time"?
①Regarding in the description
"For read-write standard command, a minimum of 2 seconds is required to get the result updated. For read-only standard commands,
there is no waiting time required, but the host must not issue any standard command more than two times per second. ",
which commands are specifically "read-write standard command" and "read-only standard commands"?
②We execute StandardCommand two times per second (reading SOC and TEMP once each).
Is there a problem against the description "the host should not issue standard commands more than once per second"?
Best Regards,
Chiaki Endo