This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL494: DUTY CYCLE ERROR IN TL494 PWM

Part Number: TL494


hello there,

                   i am using   TL494 PWM controller i have a problem with DUTY CYCLE 

my minimum duty cycle is 2.24 percent in my sample PCB  but in problem  PCB it is 3.7 percent 

and if i give light load for sample PCB say 40mA current the duty cycle raises to 0.95 percent but in problem PCB it raises to 2.61 percent

can any one suggest what would be the solution or reason in feedback circuit. 

THANKS

BHEEM