This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3880: How can i sequence more than 6 rails using LM3880

Part Number: LM3880


Hi, 

I need to sequence more than 6 rails in my system design and I am thinking to use LM3880DBV sequencer to sequence. 

How can i sequence 9 rails for ex using LM3880DBV? Do you have any application circuit?

Also in webbench if i try to sequence more than 6 rails, its not working, it just works with 6 rails always. 

Also, in the webbench report, wherein i tried to sequence 6 rails, i see one AND gate and one OR gate along with LM3880DBV. I understand AND gate is used to enable Flag4 only after Flag3 is asserted, but what is the purpose of OR gate? Attaching the schematic of the LM3880DBV given by webbench when used to sequence 6 rails.