This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53353: 5V input or 12V input are ok. output 3.3v.

Part Number: TPS53353
Other Parts Discussed in Thread: TPS53319, TPS56C230

Hi team,

My customer wants to use the TPS53353 to do the condition below.

5V input  or 12V input  are ok. output 3.3v.

We are not sure whether the device can be used here or not. i have concerns about the duty cycle and EN pin. For EN voltage rise threshold is 1.8v, we may set the EN pin 2.2v for 5V, 5.28v for 12v. Could you please help double check whether it's ok? Thanks.

They also want to try TPS53319, could you please also double check this device too?