Hi,
My customer is having an issue with residue output voltage not allowing their bq40z80 to go into shutdown when the cells go below their SUV threshold. Leakage current from their FET switch is keeping the output voltage at a level above the 2.2V min operating voltage for the device. The PACK input sees this voltage and prevents the device from going into shutdown mode.
Can they add a Zener diode in series with the PACK pin to increase the threshold from 2.2V to Zener Voltage (10V) + 2.2V?
Thanks,
Antonio