This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM25085: mosfet power loss calculation

Part Number: LM25085
Other Parts Discussed in Thread: BQ24715

Tool/software: WEBENCH® Design Tools

HI

I used webench tool to design a buck converter with the following specifications

Input: 
DC 10.1 V - 12.6 V
Output: 
9.8 V at 8 A
I calculated the mosfet power loss manually by using eq8 from the datasheet of bq24715 
While comparing the design report power loss to that of calculated one, the values are no where matching.
Can you please help in me in  calculating power loss of the mosfet?
i want to use a different mosfet in order to bring down the cost  (DMP26M7UFG-7 from diode incorporated).
Could you also tell me the change in efficiency if i go for the mosfet from diode incorporated?
I have attached the design report
Thankyou
Regards
Harini Krishna