Other Parts Discussed in Thread: BQ76PL455A-Q1, TMS320F28379D, , BQ76PL455A
Hello everyone,
As far as I understood, BQ76pl455a-q1 Evaluation Board make some measurements and transmit its measurements with Serial communication. Since we have TMS320f28379d and since this component have a MATLAB model I want to use TMS320f28379d Launch Pad. Since this will be introduction to BMS I think TMS320f283d Launch Pad will be enough for controlling Contactor and measuring current with a shunt/hall effect sensor.
The significant questions that I have in my mind are;
1. Will I be able to use both of them by connecting related TX and RX pins ? Are they in accordance to each other ?
2. I could not manage to transmit data via SCIB and SCIC on TMS320F28379d. I managed to transmit via SCIA but since it is directly connected to the USB port, I have to use another SCI for data communciation with BQ76PL455EVM. How can I use SCI other than SCIA ?
3. Normally with BQ76PL455EVM, TMS570 is recommended and a sample code presented for TMS570 ? Why there is not a Matlab embedded package for TMS 570 ?
4. Is there any TI technical person that I can call or directly send an e-mail to ask such things?
Thanks.