This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A33: Components selection

Part Number: TPS7A33

In the data sheet for the TPS7A3301RGW is states that it recommends at 0.1uF to GND ta maximize performance. 

We have in stock a CAP 1uF 10v 10%  X5R Type 0402 0402ZD105KAT2A. 

Will this be good enough ? I saw that the "NR/SS pin to GND pin : 0.3V" in the data sheets so I figured that my 10V voltage rating might be O.K.  - how ever in the development board 

C3 Capacitor, ceramic, 1 µF  50 V 0603 X5R, 10%

The problem is that we are very tight on PCB space and I need the smallest solution possible !