Hi All,
We are designing a new battery pack which would be used in a future product. This battery pack would be large, totaling at about 2000Whr. We were of the thought of making an 8S30P battery pack but issues started to come up when it came to battery management. Apart from the large currents involved, we were in doubt on how to structure the BMS for ex, should we use a single 8S BMS chip and make 8 packs of 30 cells in parallel (which I think could be dangerous having so much cells in parallel), or should we make packs of (say) 8S3P with a BMS for each pack and than use 10 packs in parallel. The later option could induce issues since we have no control on how much current each pack would be contributing.
In the end, is there anyone with experience on such battery packs which could supply some guidance and also links to white papers and applications notes?
Thanks