This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VINTANA2 Current Consumption

Other Parts Discussed in Thread: TPS65950

The VINTANA2 powers the Audi Subchip, USB Subchip and Auxillary Subchip. The maximum output current of the VINTAN2 LDO is 250mA; most of the power will be consumed by Audio subchip. The audio sub chip in the TPS65950 is not used in our application.

Do you have the VINTANA2 power consumption information with audio subchip is turned OFF. Is there any application notes available for use case power consumption calculation. Taking the worst case power consumption for all the internal LDOs gives very high power consumption eventhough the actual power consumption will be less.

  • We do not have this data and it is not a feasible experiment/use case to have this information. VINTANA2 is used by internal analog circuitry and it depends on which peripherals and settings are active at any given time.

    Due to the above reasons it is not possible to calculate VINTANA2 consumption.