This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22965: Discharge FET function

Part Number: TPS22965

 

Hi

 

Could you kindly advise the conditions that discharge FET is off ?

Our customer see the below phenomenon.

 

-        VBIAS : 5V

-        VIN : 3.3V

-        Cload : 250uF

-        CT : 500pF

 

It takes about 30 sec to drop to 0V at Vout pin even if VON is turned off.

In our understanding, Vout should be 0V for about 100m sec if discharge FET was worked properly.

 

We would much appreciate if we get your any comments.

 

Thank you and best regards,

Michiaki