This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2121: ST pin not reporting correct value

Part Number: TPS2121
The voltage is 0.0 V when IN2 is active. (This is as expected)
The voltage at pin PWR_MUX_ST is 0.78V when IN1 is active. (I expect it to be 5V)
Can anyone help as to what could be the reason?
Thanks,
Ashish