Dear Sir
our customer use BQ25896 in their new project, and find some problem when they doing EVT test.
Below table is their test result for termination current, when Ambient temperature is 45~60 degree, termination current setting is 64mA but test result is 89mA, the accuracy around 139%.
we just want to check, base on customer current setting, the termination current accuracy will over 20% or not?
If yes, what's percentage we can follow?
Thanks a lot !!
Allen