Other Parts Discussed in Thread: ULQ2004A,
Data sheet 7 pages 6.9 Electrical Characteristics: ULQ2003A and ULQ2004A
There is a notation;over recommended operating conditions (unless otherwise noted)
ULQ2003A ICEX is 100uA, what is the temperature range? -40~85℃?
If there is a full load, ULQ2004A is 85 ℃ 50uA but 70 ℃ 100uA
I am confused by the conflicting situation.
I want to know ULQ2003A's ICEX (Ta=25℃).
If you follow the notation in the data sheet, you are worried about the bad values in the ULQ200xA series