This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61160A: Selection of Current Limiting Resistor

Part Number: TPS61160A


I'm designing an LED backlight circuit needing 19.2v with 18-20ma using the TPS61160A.  Plan is to use 5v input voltage, 1uf Caps on input and output, 22uH Inductor, .22uf Comp Cap, with PWM dimming (approx 20-100%). 

My question is to verify both the resistance VALUE and POWER ratings.  Which Vfb ref do I us: Vref or Vref-pwm to calculate this?  Also, how do I calculate the power rating for this resistor?

Apologies if this is a basic question, but would appreciate the assistance.

Thanks,