This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455A-Q1: DAISY CHAIN COMMUNICATION

Part Number: BQ76PL455A-Q1

HOW DO THE BMS RESPOND TO THE DAISY CHAIN COMMUNICATION?

HOW WILL IT RETURN THE DATA WHEN SAMPLING 128 CELLS WITH 8 BMS IN THE STACK?

WILL IT BE ABLE TO GIVE ALL CELL VOLTAGES IN ONE RESPONSE FRAME?

HOW DO I TRANSMIT DATA WHEN USING MANY REGISTRES AT ONE TIME?

FOR EXAMPLE, I WANT TO USE REGISTRES 0X54 TO 0X63 (AS I DID IN ONE BMS WITHOUT DAISY CHAIN WHERE I ACCESSED ALL THESE REGISTERS IN ONE COMMAND FRAME)IN A DAISY CHAIN COMMUNICATION, HOW WILL THE RESPONSE FRAME COME OUT? WILL IT GIVE 0x54 REGISTER VALUE OF ALL THE IC's SERIALY AND THE GO FOR THE NEXT REGISTER OR WOULD IT GIVE ME ALL THE REGISTER VALUES OF THE 1st BMS IN STACK AND THEN THE OTHER?

CAN YOU GIVE ME SOME MORE EXAMPLES OF THE DAISY CHAIN COMMUNICATION FOR BROADCASTING MESSAGES TO ALL THE IC's.