This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5071: flyback transformer design for low power isolated PD

Part Number: LM5071
Other Parts Discussed in Thread: TPS23755EVM-894, TPS23754

Hello,

We are using LM5071 & LM5072-80 for small power (less than 12V/0.8A) design. Due to the mechanical limitation, we

have to use low profile transformer such as Coilcraft's ER14.5. Is there any design tool or workbench so that we can

get design parameters of flyback transformer and pass them to transformer's manufacturer? 

Best Regards,

Ben