I need a thyristor control chip so that I can output two AC signals with a phase difference of 90 degrees. Do you have any recommendation, signal ac36v 2a, thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need a thyristor control chip so that I can output two AC signals with a phase difference of 90 degrees. Do you have any recommendation, signal ac36v 2a, thank you
Hi User,
The Power Switch portfolio is designed for DC signals only. As such, I do not think these devices can be used to pass AC signals.