Hi
I want to use BQ27425-G2A and I have some issues with the layout.
In the Datasheet Figure 16 it seems you recommend a star topology with all the capacitors to VSS
but in the EVM and guidelines it looks like it is not a star topology and the VSS connected with the shortest trace.
which one is right?
Do you have the gerbers of the bq27425 EVM?
I would appreciate if you can send me the gerbers.