Hi,
Customers are considering batteries with the following specifications.
・charge voltage : 3.7V
・charge current : ~100mA
・Input voltage : 5V (by earphone cradle or case)
・40mAh cell
・2 parallel (80mAh)
Could you tell me the recommended parallel batteries charging IC and design example?
Customers have the following concerns about parallel use of batteries:
・Protection when one side of the battery comes off
・How to care for battery variations
Please introduce the best charging solution
Best Regards,
Yusuke