Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO, EV2400,
Hello,
I'm using 14S6P battery pack, the voltage of the pack when fully charged is 57.75V, the capacity of one cell is 4800mAh.
- I scaled the current of 6: used 6A actual current then calibrate it to 1A.
I set:
- Voltage divider: 57750 mV.
- I calibrated the voltage to (actual voltage/14). For example, applied voltage to the pack is 57750 mV, then the calibrated one will be 57750/14 = 4125 mV. The actual number of series cell is 14 but because I scaled voltage of 14 so I set the Number of series cell is 1.
- Design capacity: 4800 mAh.
- Design energy: 4.125V x 4800mAh = 19800 mWh.
Did I set the parameters correctly?
Thank you.