This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62420: Providing the best solution

Part Number: TPS62420
Other Parts Discussed in Thread: TPS62821, TPS62840

Hello experts,

My customer is considering DCDC converter having two outputs.

Input: 3.0V

Output: 2.0V, 500mA / 1.8V, 500mA

In addition, customer wants enable these output about a few minutes per day at the same time. Customer wants long life design.

Two channels IC is not must, is desirable.

I selected TPS62420, but there are few options in two channel DCDC converter.

Could you give me the best solutions regardless of the channel of outputs?

Best regards,

Hideki