This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suggestion for single AAA alkaline battery to 1.8v output boost converter

Other Parts Discussed in Thread: TPS61099

Hello,

We are working on Low Energy project where we are going to use single AAA alkaline battery to run whole system. And our output requirement is 1.8V with <100mA or 2.5V with <100mA current (We have not decided system voltage as of now). Also device will consume less then 10uA in sleep so, at lower power requirement efficiency  should be higher.

please suggest low Iq boost converter which suits best for our application.

Regards,

punit patel