This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65311-Q1: power up sequence

Part Number: TPS65311-Q1

Hi,

1. what is time interval between the rising edge of event and BUCK1 begin to start?just as the following picture described:

2. what is the typical value of tSTART2, in datasheet it just said that the minimum was 0.5ms and maxim was 2ms.

3. what is the typical value of tSTART, in datasheet it just said that the maxim was 3ms.

4. what is the typical value of tSEQ2, in datasheet it just said that the maxim was 3ms.

5.what is the typical value of tSEQ1, in datasheet it just said that the minimum was 1ms and maxim was 4ms.

Thanks

Best Regards.

Gavin.