This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133: BQ24133 two series battery charging abnormal

Part Number: BQ24133


Hi

BQ24133 three series battery charging, STAT is normal, the charging stat light is on, and turn off the light when charge full;

But when charging two series battery, it is normal when charging starts.

But when the voltage charge to 8.2V, the STAT light flashes. When measuring the BAT voltage jumps between 7.8v ~ 8.9V

The charging voltage has not been modified. Both three and two series are charged with 15v.
When the two series cell are charged, the cell pin is floated. When the two batteries are discharged, it is normal when charging begins. After a while, problems occurred.
Attached the schematic as below
Waiting for your reply.
Thanks
Star