This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A4101: Does it support short circuit protection?

Part Number: TPS7A4101


Hi,

     Bellow is the operation condition.Because end customer need to test short circuit protect.

Our customer want to know whthere or not  TPS7A4101 support short circuit protection?

If not could you give some advice. 

Thanks 

      Vin: 24V 

      Vout : 9V

      Iout : 50mA

  • Hi Jeff, 

    This device has the current limit protection to limit the output current during short. If the device temperature reaches 170C, the device also has thermal shutdown protection. There two protections combined should protect the device due to excessive heat at short circuit event. 

    Regards, 
    Jason Song