This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24780S: ACOK not high

Part Number: BQ24780S

Hello,

I tried to repair a laptop motherboard (internal battery failure, burned 10 Ohm Vcc resistor of the bq24780S, and a killed bq24780S device (the Vcc pin was 0 Ohm to ground instead of open line), I replaced the bq24780S with a new one and I replaced the burned 10 Ohm resistor with a new one). But when plugging the laptop adaptor, I can not get the bq24780S to have ACOK high. What am I doing wrong?  Did I kill the new bq24780S by soldering it on the motherboard (360 degrees celcius hot air soldered)?